Chris Detzel
Chris Detzel

What do I need to know about Solar panels installs?

It's a hot new trend now, and I'm thinking about adding it to my list of offerings, but I haven't done this before - anyone have any callouts or things to know about getting into solar and solar panel installations? Many thanks in advance!

  • There are general requirements to become a certified Solar PV installer.

    To be eligible to become a qualified solar installation and design professional you must:

    1. Be at least 18 years old

    2. Complete 18 hours of training with a NABCEP Entry Level Exam Provider

    3. Successfully pass the NABCEP Entry Level Exam

    4. Complete 40 hours of Advanced Training hours

    5. Receive an OSHA 10 hour card

    6. Be the lead installer on 3-5 solar photovoltaic installs

    7. Pass the NABCEP PV Installation Professional certification exam

    General information on certification and testing can be found here: http://www.nabcep.org/

    For a list of USA and Canada Certified Installer, click here: http://www.nabcep.org/certified-installer-locator

    Another great site for guidance on becoming a solar installer can be found here: www.solarenergy.org

    Our WebShop contains all of our current offerings, both in-stock and direct ships.

    Contact us @ 1-855-REX-SOLAR (739-76527) for assistance with product recommendations, logistics questions, availability, pricing or general technical support.

    SolarSolutions@RexelUSA.com

    For examples of sales proposals and how contractors can create them on their own, guide them to RexelPRO, www.RexelPRO.com, for a 30 Day FREE Trial.

  • Chris Detzel
    Chris Detzel

    Als Antwort auf Marty Yudice:

    Thanks ! So, assuming I can be the lead (#6) if I have completed tasks 1-5? Appreciate it.
  • To see where it is, determine the elevation of the solar panel according to the dimension of the geographic location. It is not about 10 degrees in the southwest of the tracking system, but also a reliable grounding and lightning protection. In addition, the solar cell board is determined by the voltage of your system.
Verwandt Posts