Buy Abortion pills in Abu Dhabi, Dubai, Muscat, Doha, Riyahd and Dammam WhatsApp +1(802)468-7218.

CONTACT US!!!!!
WhatsApp Number: +1(802)468-7218

The Women’s Center of Hyde Park (Tampa Abortion Clinic) was established in 1998 and is located in the beautiful, Lakeshore District of Hyde Park in Tampa Bay. It has been serving the State of FLorida and the United States for over 20 years.

Our Abu Dhabi, United Arab Emirates Abortion Clinic provides the safest and most advanced techniques for providing non-surgical, medical and surgical abortion methods for early through late second trimester, including the Abortion By Pill Procedure (RU 486, Mifeprex, Mifepristone, early options French Abortion Pill), Tamoxifen, Methotrexate and Cytotec (Misoprostol).

The Abu Dhabi, United Arab Emirates Abortion Clinic performs Same Day Abortion Procedure using medications that are taken on the first day of the office visit and will cause the abortion to occur generally within 4 to 6 hours (as early as 30 minutes) for patients who are 3 to 12 weeks pregnant.

When Mifepristone and Misoprostol are used, 50% of patients complete in 4 to 6 hours; 75 to 80% in 12 hours; and 90% in 24 hours. We use a regimen that allows for completion without the need for surgery 99% of the time.

All advanced second trimester and late term pregnancies at our Tampa clinic (17 to 24 weeks or greater) can be completed within 24 hours or less 99% of the time without the need of surgery. The procedure is completed with minimal to no complications.

Our Women’s Health Center located in Abu Dhabi, United Arab Emirates, Abu Dhabi, United Arab Emirates, uses the latest medications for medical abortions (RU486, Mifeprex, Mifegyne, Mifepristone, early options French abortion pill), Methotrexate and Cytotec (Misoprostol).

The safety standards of our Abu Dhabi, United Arab Emirates Abortion Doctors remain unparalleled. They consistently maintain the lowest complication rates throughout the nation.

Our Physicians and staff are always available to answer questions and care for women in one of the most difficult times in their life.

The decision to have an abortion at the Abortion Clinic in Abu Dhabi, United Arab Emirates, involves moral, ethical, religious, family, financial, health and age considerations.

WhatsApp +1(802)468-7218.

Related Posts