Registered Users Member

C16 circuit breaker

How many light (CFL) need on the c16 circuit breaker?

  • Registered Users Member
    ● Rated DC operating voltage - higher than the highest AC peak voltage (220V): 400VDC ~ 450VDC (APFC circuit);
    ● Capacitance and deviation - electronic energy-saving lamp (CFL): 4.7 ~ 10μF; electronic ballast: 20 ~ 40W, 10 ~ 22μF; > 40W, 22 ~ 47μF; allowable capacitance deviation ± 20%; filter capacitor capacity is not appropriate too small

    If you want to buy C16, you can visit: www.winsupport-ic.com/.../C16.html
Related Posts