Registered Users Member

Is There Any Best LED Light?

I have seen so many people asking this question so I thought it would be nice to talk a bit about it. In my opinion, there’s no “best” without knowing what you want. Lots of light as cheaply as possible? Or the closest you can get to daylight? Or the closest you can get to an old-style filament bulb?

For lots of light as cheaply as possible you concentrate on the lumens/Watt rating.

For the best quality light you concentrate on the CRI (a.k.a. Ra) rating. A halogen bulb is rated 100. The best LEDs are 98. Good is 95. The typical cheap supermarket ones say “greater than 80”, which is basically crap. CFL lights were/are 80. Philips and Osram also say “greater than 80” but are somewhat nicer, so presumably somewhat more greater than the others. But why not actually give a specification?

For daylight versus lightbulb effect you concentrate on the colour temperature. 2700K is like an old light-bulb, 3000K more like a halogen bulb, 4000K much like daylight (but at night it looks far too “blue” to me, and may even disrupt your sleep patterns).

If I’m replacing a spotlight (GU10) or ordinary bulb (bayonet or ES) in a room where I live and work, I’ll seek out the highest CRI and prefer 2700K. Although the bulb will be expensive, it’ll still save its purchase cost in electricity inside the first couple of years.

CV Light is one brand of high-CRI bulbs available in the UK.

  • Finolex LED lighting range offeres a wide range of best quality products which are efficient, environment-friendly and long-lasting. Designed to the highest quality specification, the Finolex LED products are ideal for domestic and industrial user as well. The Retrofit bulb-shaped LED in 0.5W Deco is in five colours in various wattage specifications ranging from 3W-12W. Indoor lighting includes LED Flat Panel Down Lighters ranging from 6W-24W and LED Slim tubelight fixture in specifications of 5W, 10W, &18W (Available in 6500K & 3000K). Street lights ranging from 10W – 210W and industrial High Bay Fixtures ranging from 45W – 210W are also available. Finolex LED tubelight fixture available in 5W, 10W & 18W having very high lumen output.

     

    ___________________________________________________________________________________

    I have use moon lamps here and I think this is the best lamps for home use and many more.

     
  • Registered Users Member
    And what do you think about lamps that change their warmth? Is it a good idea, os it rational?
  • I have no idea about it. But I am planning to get LED lights installed in my house. It would be great if I get some suggestions for the best LED lights.

  • In reply to JohnTowns:

    Either will work fine. I would choose the cheaper, lower power nano for a task that does not require a lot of best led garage lights and does not require intense processing power. The nano does have 2 additional analog inputs though, not needed for a distance sensor.

  • Registered Users Member

    In reply to darensammy352310:

    I have some suggestions for you to the choose best Led and Light you can read about some review here <A href="davegaubatz.com/.../">Best Light</a>
  • Registered Users Member

    In reply to sevelina:

    These 5 are top Brands for LED lights:
    I am using Philips Sceneswitch at my Home. It's a little bit Costly but once you get it you have to spent 0 pence till 5 years.
    Philips SceneSwitch 60W Equivalent LED. Best LED for Versatility.
    Philips 464487 Hue White and Color Ambiance A19 60W. Best Smart LED.
    SYLVANIA 60W Equivalent Soft White Bulb. Best Budget LED.
    Sunco Lighting Dimmable Flood Light LED. Best Outdoor LED.
    Feit Electric 6.5W Vintage Style LED
  • Registered Users Member
    i saw that https://ndrelectric.com, have some lightning solutions
Related Posts