Registered Users Member

Hp Designjet T120 featurepacked device

The Fit to Paper function in an Hp Designjet T120 is a differentiating feature. If the paper size is smaller than the selected paper size, the driver reduces the print size. If the paper size is larger than the size of the document to be printed, the print job is not adjusted to fit the paper size. This is one of a kind feature that is unavailable in the other laserjet devices in the segment.

Related Posts