Single Mode Fiber Optic Cable

What are the typical transmission speed and distance limits for single mode fiber optic cable?

  • Cisco is brilliant with this kind of information. Westburne can buy Cisco items.

    I hope these two references help.

    www.cisco.com/.../tech_brief09186a0080091a8a.html

    Single-mode fiber has been traditionally used in the networking cable plants to achieve long distance. In Ethernet, for example, single-mode cable ranges reach up to 10 km. Single-mode fiber, using a 9-micron core and 1300-nanometer laser, demonstrates the longest distance technology. The small core and lower-energy laser elongate the wavelength of the laser and allow it to transverse greater distances. This setup enables single-mode fiber to reach the greatest distances of all media with the least reduction in noise

    www.cisco.com/.../tech_brief09186a0080091a8a.html

    LH GBICs extended the single-mode fiber distance from the standard 5 km to 10 km.

    One of the delays with 802.3z was with solving the problem of differential mode delay (DMD). DMD affects only multimode fiber when using SX lasers. The problem is when one mode of light experience jitters (line distortion), this could, in extreme cases, cause a single mode to be divided into two or more modes of light (see Figure 7). In other words, data would be lost. Multimode fiber was designed for short-distance light emitting diodes (LEDs), not lasers.
  • Hi AaronBerlinic,
    Single mode is much better in many ways. It is the popular mode for longer transmissions. It also gives more bandwidth than multi-mode. So it has also greater speed than multi fiber. Companies usually use it for longer distances to provide the best signal strength like a Homeinternetprovider.com. So it will give you a better experience if you are getting the services in the far away area.

  • did this answer your question?
  • Let us know if you have any other questions!
     
  • Typical multi-mode links have data rates of 10 Mbit/s to 10 Gbit/s over link lengths of up to 600 meters (2000 feet). Multi-mode fiber has a fairly large core diameter that enables multiple light modes to be propagated and limits the maximum length of a transmission link because of modal dispersion. You might as well ask for sufficient mechanical strenght loads for a help.

Verwandt Posts